Dialog 'Options' – 'International Settings'Permanentlink

Symbol: _cds_icon_options_int_set

Funktion: This dialog is for the setting of the language in the user interface and in the help.

Rufen Sie an: Menüleiste: „Tools  Options“, category „International Settings“.

Tab 'User Interface Language'

Same as Microsoft Windows

_cds_icon_option_activated The language is taken from the Microsoft Windows settings.

Specific language

_cds_icon_option_deactivated

  • Deutsch

  • English

  • espanol

  • francais

  • chinese

Changing the user interface language will not bee effective until this application is restarted. Some components may not be available in the selected language and will then appear in their default culture (typically in English).